Leverage Analysis
Through leverage analysis it is possible to observe which adjustable variables offer the most leverage for correcting a process deviation.
As with the cause analysis, the leverage analysis view can be loaded from the main toolbar.
On the leverage graph red bars indicate the relative influence that the input will have on the model output if increased, and the blue bars indicate the relative influence if the input is decreased.
Related topics: